SWO Trace functions without SWO connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SWO Trace functions without SWO connection

2,194 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Apr 01 06:08:40 MST 2015
Obviously it's possible to use SWO trace without SWO connection  :~

Is there any kind of summery which SWO Trace functions are working without SDO connection?

Something like:

Function - SWO connection required
-----------------------------------------------------
SWO DATA - No
SWO Counters - Yes

Note. Target is LPC1549
0 Kudos
Reply
4 Replies

2,105 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Apr 01 07:04:19 MST 2015
Thanks for clarifying.
0 Kudos
Reply

2,105 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Apr 01 06:58:57 MST 2015
OK, I had forgotten about that.

The data monitor (as this feature is called) does not use any trace functionality and works by polling the memory location (using the standard debug connection). As mentioned, this is a Technology Preview, and this is one of the areas where the UI will be changing.
0 Kudos
Reply

2,105 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Apr 01 06:39:23 MST 2015
So this part of SWO Data is not using SWD Trace  :quest:

[img=388x388]http://www.lpcware.com/system/files/SWO.JPG[/img]

0 Kudos
Reply

2,105 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Apr 01 06:18:30 MST 2015
To use any of the SWO Trace facilities, as released in  LPCXpresso 7.7.2, the SWV pin (also referred to as SWO on some chips and board)  must be connected (as described here: http://www.lpcware.com/content/faq/lpcxpresso/debug-design).

Note: Ensure you read the FAQ http://www.lpcware.com/content/faq/lpcxpresso/trace-overview which describes any part specific setup.
0 Kudos
Reply