Run from menu LPCXpresso 6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Run from menu LPCXpresso 6

2,677件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Tue Oct 29 17:46:45 MST 2013
Hi,

With LPCXpresso 6.x is not possible to launch the application, unless you select: open the console.

openSUSE.

Thank you.
0 件の賞賛
返信
5 返答(返信)

2,669件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by elektronist on Wed Oct 30 11:41:45 MST 2013
Same here for Rosa Linux.

For menu entry I use your solution too.

If /usr/local/lpcxpresso_6.0.4_159/lpcxpresso/lpcxpresso clicked in Dolphin, program runs with no problem. (as user)

But this is the good. The bad is with updated webkit1.0-2.0.4 package there is no way to run lpcxpresso. I have to downgrade to webkit1.0-1.10.0.





0 件の賞賛
返信

2,667件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Wed Oct 30 08:49:02 MST 2013
I'm trying to run LPCXpresso from the menu. The program starts to load, but then stops, no errors.

If I select run in terminal (kmenuedit), then it works.
0 件の賞賛
返信

2,667件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Wed Oct 30 08:41:42 MST 2013

Quote: vilserg
"open the console" means with root rights?

No.
0 件の賞賛
返信

2,667件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vilserg on Wed Oct 30 08:27:49 MST 2013
"open the console" means with root rights?
0 件の賞賛
返信

2,667件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Oct 29 21:04:12 MST 2013
Sorry, but I have no idea what you are referring to.

Perhaps you explain what you are trying to do and what you think is wrong, and why.
0 件の賞賛
返信