RedState editor for LPC43S67 support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RedState editor for LPC43S67 support

Jump to solution
1,116 Views
javiervallori
Contributor III

Hi,

I'm trying to use the SCT module of a LPC43S67. The LPCXpresso has a RedState editor integrated, but in the "target" field on State Machine Settings, it does not appear the LPC43S67 model, even when it has this module. Is there any solution for it? Thank you

Labels (1)
Tags (3)
1 Solution
976 Views
lpcxpresso_supp
NXP Employee
NXP Employee

You can just select LPC4357 within RedState. The LPC4367 is a LPC4357 with a 2nd Cortex-M0 cpu, and the "S" is not relevant for Redstate/SCT usage.

Regards,

LPCXpresso Support

View solution in original post

1 Reply
977 Views
lpcxpresso_supp
NXP Employee
NXP Employee

You can just select LPC4357 within RedState. The LPC4367 is a LPC4357 with a 2nd Cortex-M0 cpu, and the "S" is not relevant for Redstate/SCT usage.

Regards,

LPCXpresso Support