RedState editor for LPC43S67 support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RedState editor for LPC43S67 support

ソリューションへジャンプ
1,694件の閲覧回数
javiervallori
Contributor III

Hi,

I'm trying to use the SCT module of a LPC43S67. The LPCXpresso has a RedState editor integrated, but in the "target" field on State Machine Settings, it does not appear the LPC43S67 model, even when it has this module. Is there any solution for it? Thank you

ラベル(1)
タグ(3)
1 解決策
1,554件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

You can just select LPC4357 within RedState. The LPC4367 is a LPC4357 with a 2nd Cortex-M0 cpu, and the "S" is not relevant for Redstate/SCT usage.

Regards,

LPCXpresso Support

元の投稿で解決策を見る

1 返信
1,555件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

You can just select LPC4357 within RedState. The LPC4367 is a LPC4357 with a 2nd Cortex-M0 cpu, and the "S" is not relevant for Redstate/SCT usage.

Regards,

LPCXpresso Support