ROM USB CDC example for LPC1347

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ROM USB CDC example for LPC1347

606件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by AchimKraus on Mon Feb 17 04:59:36 MST 2014
Hallo,

I tried to understand the ROM USB CDC example in „NXP_LPC1347_2012_02_22.zip“ from LPCXpresso 6.1.4_194_Linux-x86 for the LPC1347. Studying the source makes me wonder:

1. line 381 in main.c
   /* initilize call back structures */
   memset((void*) &usb_param, 0, sizeof(USBD_API_INIT_PARAM_T));
   usb_param.usb_reg_base = LPC_USB_BASE;
   usb_param.mem_base = 0x10001000;
   usb_param.mem_size = 0x1000;

0x10001000 points into the middle of the 8K SRAM, right? And there is no need to protect this area from being used in an other way? Or does this simple example just probably not use this memory?

2. Is it possible to use the 2K USB SRAM with
   
   usb_param.mem_base = 0x20004000; // RAM
   usb_param.mem_size = 0x800; // 2K;
  
   or is that area reserved for an internal use of the USB?

3. line 427 in main.c
   
   /* allocate transfer buffers */
   g_vCOM.rxBuf = (uint8_t*) (cdc_param.mem_base
+ (0 * USB_HS_MAX_BULK_PACKET));
   g_vCOM.txBuf = (uint8_t*) (cdc_param.mem_base
+ (1 * USB_HS_MAX_BULK_PACKET));
   cdc_param.mem_size -= (4 * USB_HS_MAX_BULK_PACKET);
      
   Is it really possible to use those buffer, which are passed in as parameter to hw->init and cdc->init?
   Which effect has altering the mem_size? Must the mem_base be adjusted as well?

I just search the forum but I may have missed the already given information on that issues.
So would alos be glad to be pointed to already given answers.

Thanks and best regards
Achim 
0 件の賞賛
返信
0 返答(返信)