Programming time

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Programming time

566 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Brinkand on Thu Jun 03 01:04:48 MST 2010
I am developing a platform which is to support both LPC1111 and LPC1311, and therefore it would be nice to be able to program both using the boothloader via the UART. I tried this using Flash Magic, and setting the High speed communication flag and max baud = 230400, it takes 30 seconds to program the LPC1114 (entire flash programmed = fill unused flash flag set.) Based on flash size, LPC1111 and LPC1311 would be 7.5 seconds (neglecting overhead).

Have anybody found ways to reduce programming time further than this?

Time is money for a production environment.
0 项奖励
回复
0 回复数