Programming time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming time

554件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Brinkand on Thu Jun 03 01:04:48 MST 2010
I am developing a platform which is to support both LPC1111 and LPC1311, and therefore it would be nice to be able to program both using the boothloader via the UART. I tried this using Flash Magic, and setting the High speed communication flag and max baud = 230400, it takes 30 seconds to program the LPC1114 (entire flash programmed = fill unused flash flag set.) Based on flash size, LPC1111 and LPC1311 would be 7.5 seconds (neglecting overhead).

Have anybody found ways to reduce programming time further than this?

Time is money for a production environment.
0 件の賞賛
返信
0 返答(返信)