Programm/errase errors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programm/errase errors

1,050 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ArtjomGromak on Thu Nov 10 11:43:39 MST 2011
Hi!
I can't program or erase LPC1114 with LPCXpresso.
The error text:


Quote:

Pc: (  0) Reading remote configuration
Ni: LPCXpresso Debug Driver v4.0 (Sep 21 2011 20:05:54)
Nc: Looked for chip XML file in C:/nxp/LPCXpresso_4.1.0_190/lpcxpresso/bin/LPC1114/302.xml

Nc: Looked for vendor directory XML file in C:/nxp/LPCXpresso_4.1.0_190/lpcxpresso/bin/nxp_directory.xml

Nc: Found generic directory XML file in C:/nxp/LPCXpresso_4.1.0_190/lpcxpresso/bin/crt_directory.xml

Pc: (  5) Remote configuration complete
Pc: ( 30) Emulator Connected
Pc: ( 40) Debug Halt
Pc: ( 50) CPU ID
Nc: Emu(0): Conn&Reset. DpID:  BB11477. Info: T1S6RGRIA
Nc: SWD Frequency: 250 KHz. RTCK: False. Vector catch: False.
Nc: Packet delay: 0  Poll delay: 0.
Xl:
Xc:
Wc: IAPExecute Error: Ef(9). Flash erase or write operation aborted.

Nc: NXP: LPC1114/302  Part ID: 0x00000000
Pc: ( 65) Chip Setup Complete
Nt: Connected: was_reset=false. was_stopped=true
Cr:v Registered license, download limit of 128K
Pc: ( 70) License Check Complete
Nt: Mass Erase
Xl:
Xc:
Wc: IAPExecute Error: Ef(9). Flash erase or write operation aborted.

Ed:04: Failed to erase flash: Ef(9). Flash erase or write operation aborted.
Pc: (100) Target Connection Failed


[ATTACH]585[/ATTACH]

What does this error mean?
What it is possible to do with CPU?
thanks
0 Kudos
Reply
2 Replies

1,026 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ArtjomGromak on Thu Nov 10 12:16:13 MST 2011

Quote: Zero

Could you program / debug it before?

http://support.code-red-tech.com/CodeRedWiki/DebugAccessChip


Yes, debugged on this board earlier.


Quote: Zero

Did you try Vector catch and ISP already?

http://support.code-red-tech.com/CodeRedWiki/DebugAccessChip



Thanks for the help, Zero. All again works.
0 Kudos
Reply

1,026 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Nov 10 11:53:00 MST 2011
Could you program / debug it before?

Did you try Vector catch and ISP already?

http://support.code-red-tech.com/CodeRedWiki/DebugAccessChip
0 Kudos
Reply