Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem

4,073 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andrei.badila on Fri Sep 07 02:53:56 MST 2012
I'm use NXP LPC1114 and Any program that I want to write on the board gives me : Errror launching Debug\xxx.axf
02: Failed on connect : Ee(07). Bad Ack returned from status -wire error.:
I mention that I changed cable, USB port and same problem.
Also mention that after I wrote the following program on board began to show error.
Some ideea? Thanks very much!
void SSP_LoopbackTest( uint8_t portNum )
{
  uint32_t i;

  if ( portNum == 0 )
  {
  while(1){
#if !USE_CS
  /* Set SSEL pin to output low. */
  GPIOSetValue( PORT0, 2, 0 );
  GPIOSetValue( PORT0, 2, 1 );
  for ( i = 0; i < 0x25; i++ );
  GPIOSetValue( PORT0, 2, 0 );
#endif
  i = 0;
  src_addr[0]=0x12;
  src_addr[1]=0xFF;
  while ( i <= SSP_BUFSIZE )
  {
/* to check the RXIM and TXIM interrupt, I send a block data at one time
based on the FIFOSIZE(8). */

  SSP_Send( portNum, (uint8_t *)&src_addr, FIFOSIZE );
/* If RX interrupt is enabled, below receive routine can be
also handled inside the ISR. */
//  SSP_Receive( portNum, (uint8_t *)&dest_addr, FIFOSIZE );
i += FIFOSIZE;
  }
#if !USE_CS
  /* Set SSEL pin to output high. */
  GPIOSetValue( PORT0, 2, 1 );
#endif
  }}
  else
  {
#if !USE_CS
/* Set SSEL pin to output low. */
GPIOSetValue( PORT2, 0, 0 );
#endif
i = 0;
while ( i <= SSP_BUFSIZE )
{
  /* to check the RXIM and TXIM interrupt, I send a block data at one time
  based on the FIFOSIZE(8). */
  SSP_Send( portNum, (uint8_t *)&src_addr, FIFOSIZE );
  /* If RX interrupt is enabled, below receive routine can be
  also handled inside the ISR. */
  SSP_Receive( portNum, (uint8_t *)&dest_addr, FIFOSIZE );
  i += FIFOSIZE;
}
#if !USE_CS
/* Set SSEL pin to output high. */
GPIOSetValue( PORT2, 0, 1 );
#endif
  }
  return;
}

/*****************************************************************************
** Function name:SEEPROMTest
**
** Descriptions:Serial EEPROM(Atmel 25xxx) test
**
** parameters:port #
** Returned value:None
**
*****************************************************************************/
void SSP_SEEPROMTest( uint8_t portNum )
{
  uint32_t i, timeout;

  if ( portNum == 0 )
  {
  LPC_IOCON->PIO0_2 &= ~0x07;/* SSP SSEL is a GPIO pin */
  GPIOSetValue( PORT0, 2, 1 );
  /* port0, bit 2 is set to GPIO output and high */
  GPIOSetDir( PORT0, 2, 1 );
 
  GPIOSetValue( PORT0, 2, 0 );
  /* Test Atmel 25016 SPI SEEPROM. */
  src_addr[0] = WREN;/* set write enable latch */
SSP_Send( portNum, (uint8_t *)src_addr, 1 );
  GPIOSetValue( PORT0, 2, 1 );

  for ( i = 0; i < DELAY_COUNT; i++ );/* delay minimum 250ns */

  GPIOSetValue( PORT0, 2, 0 );
  src_addr[0] = RDSR;/* check status to see if write enabled is latched */
SSP_Send( portNum, (uint8_t *)src_addr, 1 );
SSP_Receive( portNum, (uint8_t *)dest_addr, 1 );
  GPIOSetValue( PORT0, 2, 1 );
if ( (dest_addr[0] & (RDSR_WEN|RDSR_RDY)) != RDSR_WEN )
  /* bit 0 to 0 is ready, bit 1 to 1 is write enable */
  {
while ( 1 );
  }

  for ( i = 0; i < SSP_BUFSIZE; i++ )/* Init RD and WR buffer */   
  {
src_addr[i+3] = i;/* leave three bytes for cmd and offset(16 bits) */
dest_addr = 0;
  }

  /* please note the first two bytes of WR and RD buffer is used for
  commands and offset, so only 2 through SSP_BUFSIZE is used for data read,
  write, and comparison. */
  GPIOSetValue( PORT0, 2, 0 );
  src_addr[0] = WRITE;/* Write command is 0x02, low 256 bytes only */
  src_addr[1] = 0x00;/* write address offset MSB is 0x00 */
  src_addr[2] = 0x00;/* write address offset LSB is 0x00 */
SSP_Send( portNum, (uint8_t *)src_addr, SSP_BUFSIZE );
  GPIOSetValue( PORT0, 2, 1 );

  for ( i = 0; i < 0x30000; i++ );/* delay, minimum 3ms */
 
  timeout = 0;
  while ( timeout < MAX_TIMEOUT )
  {
GPIOSetValue( PORT0, 2, 0 );
src_addr[0] = RDSR;/* check status to see if write cycle is done or not */
  SSP_Send( portNum, (uint8_t *)src_addr, 1);
  SSP_Receive( portNum, (uint8_t *)dest_addr, 1 );
GPIOSetValue( PORT0, 2, 1 );
if ( (dest_addr[0] & RDSR_RDY) == 0x00 )/* bit 0 to 0 is ready */
{
    break;
}
timeout++;
  }
  if ( timeout == MAX_TIMEOUT )
  {
while ( 1 );
  }

  for ( i = 0; i < DELAY_COUNT; i++ );/* delay, minimum 250ns */

  GPIOSetValue( PORT0, 2, 0 );
  src_addr[0] = READ;/* Read command is 0x03, low 256 bytes only */
  src_addr[1] = 0x00;/* Read address offset MSB is 0x00 */
  src_addr[2] = 0x00;/* Read address offset LSB is 0x00 */
SSP_Send( portNum, (uint8_t *)src_addr, 3 );
SSP_Receive( portNum, (uint8_t *)&dest_addr[3], SSP_BUFSIZE-3 );
  GPIOSetValue( PORT0, 2, 1 );
  }
  else/* Port 1 */
  {
LPC_IOCON->PIO2_0 &= ~0x07;/* SSP SSEL is a GPIO pin */
GPIOSetValue( PORT2, 0, 1 );
/* port0, bit 2 is set to GPIO output and high */
GPIOSetDir( PORT2, 0, 1 );

GPIOSetValue( PORT2, 0, 0 );
/* Test Atmel 25016 SPI SEEPROM. */
src_addr[0] = WREN;/* set write enable latch */
SSP_Send( portNum, (uint8_t *)src_addr, 1 );
GPIOSetValue( PORT2, 0, 1 );

for ( i = 0; i < DELAY_COUNT; i++ );/* delay minimum 250ns */

GPIOSetValue( PORT2, 0, 0 );
src_addr[0] = RDSR;/* check status to see if write enabled is latched */
SSP_Send( portNum, (uint8_t *)src_addr, 1 );
SSP_Receive( portNum, (uint8_t *)dest_addr, 1 );
GPIOSetValue( PORT2, 0, 1 );
if ( (dest_addr[0] & (RDSR_WEN|RDSR_RDY)) != RDSR_WEN )
/* bit 0 to 0 is ready, bit 1 to 1 is write enable */
  {
  while ( 1 );
}

for ( i = 0; i < SSP_BUFSIZE; i++ )/* Init RD and WR buffer */   
{
  src_addr[i+3] = i;/* leave three bytes for cmd and offset(16 bits) */
  dest_addr = 0;
}

/* please note the first two bytes of WR and RD buffer is used for
commands and offset, so only 2 through SSP_BUFSIZE is used for data read,
write, and comparison. */
GPIOSetValue( PORT2, 0, 0 );
src_addr[0] = WRITE;/* Write command is 0x02, low 256 bytes only */
src_addr[1] = 0x00;/* write address offset MSB is 0x00 */
src_addr[2] = 0x00;/* write address offset LSB is 0x00 */
SSP_Send( portNum, (uint8_t *)src_addr, SSP_BUFSIZE );
GPIOSetValue( PORT2, 0, 1 );

for ( i = 0; i < 0x30000; i++ );/* delay, minimum 3ms */
 
timeout = 0;
while ( timeout < MAX_TIMEOUT )
  {
  GPIOSetValue( PORT2, 0, 0 );
  src_addr[0] = RDSR;/* check status to see if write cycle is done or not */
  SSP_Send( portNum, (uint8_t *)src_addr, 1);
  SSP_Receive( portNum, (uint8_t *)dest_addr, 1 );
  GPIOSetValue( PORT2, 0, 1 );
  if ( (dest_addr[0] & RDSR_RDY) == 0x00 )/* bit 0 to 0 is ready */
  {
break;
  }
  timeout++;
  }
if ( timeout == MAX_TIMEOUT )
  {
  while ( 1 );
}

for ( i = 0; i < DELAY_COUNT; i++ );/* delay, minimum 250ns */

GPIOSetValue( PORT2, 0, 0 );
src_addr[0] = READ;/* Read command is 0x03, low 256 bytes only */
src_addr[1] = 0x00;/* Read address offset MSB is 0x00 */
src_addr[2] = 0x00;/* Read address offset LSB is 0x00 */
SSP_Send( portNum, (uint8_t *)src_addr, 3 );
SSP_Receive( portNum, (uint8_t *)&dest_addr[3], SSP_BUFSIZE-3 );
GPIOSetValue( PORT2, 0, 1 );
  }
  return;
}

/******************************************************************************
**   Main Function  main()
******************************************************************************/
int main (void)
{
  uint32_t i;
#if SSP_DEBUG
  int8_t temp[2];
#endif

  SystemInit();

#if SSP_DEBUG
  UARTInit(115200);
#endif

  SSP_IOConfig( SSP_NUM );/* initialize SSP port, share pins with SPI1
on port2(p2.0-3). */
  SSP_Init( SSP_NUM );

  for ( i = 0; i < SSP_BUFSIZE; i++ )
  {
src_addr = (uint8_t)i;
dest_addr = 0;
  }

#if TX_RX_ONLY
  /* For the inter-board communication, one board is set as
  master transmit, the other is set to slave receive. */
#if SSP_SLAVE
  /* Slave receive */
  SSP_Receive( SSP_NUM, (uint8_t *)dest_addr, SSP_BUFSIZE );
  for ( i = 0; i < SSP_BUFSIZE; i++ )
  {
if ( src_addr != dest_addr )
{
  while ( 1 );/* Verification failure, fatal error */
}
  }
#else
  /* Master transmit */
  SSP_Send( SSP_NUM, (uint8_t *)src_addr, SSP_BUFSIZE);
#endif
#else
  /* TX_RX_ONLY=0, it's either an internal loopback test
  within SSP peripheral or communicate with a serial EEPROM. */
#if LOOPBACK_MODE
  SSP_LoopbackTest( SSP_NUM );
#else
  SSP_SEEPROMTest( SSP_NUM );
  /* If SW CLK is used as SSP clock, change the setting before
  serial EEPROM test, restore after the test. */
#ifdef __JTAG_DISABLED
  LPC_IOCON->SWCLK_PIO0_10 &= ~0x07;/* Restore SWD CLK */
#endif 
#endif/* endif NOT LOOPBACK_MODE */
#if LOOPBACK_MODE
  for ( i = 0; i < SSP_BUFSIZE; i++ )
#else
  /* for EEPROM test, verifying, ignore the difference in the first
  three bytes which are used as command and parameters. */
  for ( i = 3; i < SSP_BUFSIZE; i++ )
#endif
  {
if ( src_addr != dest_addr )
{
#if SSP_DEBUG
  temp[0] = (dest_addr & 0xF0) >> 4;
  if ( (temp[0] >= 0) && (temp[0] <= 9) )
  {
temp[0] += 0x30;
  }
  else
  {
temp[0] -= 0x0A;
temp[0] += 0x41;
  }
  temp[1] = dest_addr & 0x0F;
  if ( (temp[1] >= 0) && (temp[1] <= 9) )
  {
temp[1] += 0x30;
  }
  else
  {
temp[1] -= 0x0A;
temp[1] += 0x41;
  }
  UARTSend((uint8_t *)&temp[0], 2);
  UARTSend("\r\n", 2);
#endif
  while( 1 );/* Verification failed */
}
  }
#if SSP_DEBUG
  UARTSend("PASS\r\n", 6);
#endif
#endif/* endif NOT TX_RX_ONLY */
  return 0;
}

/******************************************************************************
**                            End Of File
******************************************************************************/
0 项奖励
回复
15 回复数

4,017 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andrei.badila on Thu Sep 13 14:54:33 MST 2012

Quote: Zero
This is a CMSIS 2.0 project and including ${workspace_loc:/CMSISv2p00_LPC11xx/inc} ;)



Thx very much
0 项奖励
回复

4,017 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Sep 13 14:47:50 MST 2012
This is a CMSIS 2.0 project and including ${workspace_loc:/CMSISv2p00_LPC11xx/inc} ;)
0 项奖励
回复

4,017 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andrei.badila on Thu Sep 13 13:22:17 MST 2012
I download your project and the compilator not found this header
#include "system_LPC11xx.h"

DescriptionResourcePathLocationType
fatal error: system_LPC11xx.h: No such file or directorycr_startup_lpc11.c/LPC11_SPI_4_dummies/srcline 51C/C++ Problem
0 项奖励
回复

4,017 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Sep 13 11:51:50 MST 2012
Use Sample in #14 http://knowledgebase.nxp.com/showthread.php?t=2372 to learn how SSP is working ;)
0 项奖励
回复

4,017 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andrei.badila on Thu Sep 13 11:12:52 MST 2012
Hi Zero,
I have new problem.
I want to comunicate by bus spi with da1 module. My problem is i dont know what spi port to use. I use port 1 and 0, and i conect osciloscope to my board( pin mosi , ssel, sck) and this pin not change.
Please give me a ideea thx
0 项奖励
回复

4,017 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andrei.badila on Sat Sep 08 08:19:47 MST 2012
Thank's for all zero:)! I confused ISP pin with RST pin.:D
0 项奖励
回复

4,017 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Sep 07 19:56:15 MST 2012
TeamViewer can't help to switch to ISP :rolleyes:

This video describes how to switch your board to ISP: http://youtu.be/chFv1EiZcYohttp://http://youtu.be/3sqpPYe2RCs
0 项奖励
回复

4,017 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andrei.badila on Fri Sep 07 08:57:39 MST 2012
I want to instal teem viewer and give full acces to my computer, plese tel  if you agreea. My skype name is simionandrei.badila
0 项奖励
回复

4,017 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andrei.badila on Fri Sep 07 06:46:12 MST 2012
I font the st, i found the rst, and have conection and release, rezolts some problem
0 项奖励
回复

4,017 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Sep 07 06:32:53 MST 2012

Quote: andrei.badila
The photo of the bord is here

http://dl.transfer.ro/photo-transfer_ro-07sep-76ab2b.rar



And there: http://www.embeddedartists.com/sites/default/files/image/product/xpr_lpc1114.png

And there: http://www.embeddedartists.com/products/lpcxpresso/lpc1114_xpr.php

Where you can also find the schematic link I've posted already :)
0 项奖励
回复

4,017 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andrei.badila on Fri Sep 07 06:24:54 MST 2012
I have assert gnd to rst, release, and some problem.
0 项奖励
回复

4,017 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andrei.badila on Fri Sep 07 06:14:39 MST 2012
The photo of the bord is here

http://dl.transfer.ro/photo-transfer_ro-07sep-76ab2b.rar
0 项奖励
回复

4,017 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Sep 07 06:07:24 MST 2012
Then try Google:

Quote:

Asta este, GND pini ISP-ul, afirma RST, apoi scoate?i GND la ISP pini. Dupa ce în bootloader ISP-ul, configurare ceasul ?inta este stabila, iar pinii de depanare sunt în starea implicita a acestora - ar trebui sa fie în masura sa se conecteze.
Nota: PIN-ul ISP este: P0.1 - pentru LPC11xx ?i LPC13xx

So just ground ISP pin, reset your board, release ISP pin and try to debug again.

ISP pin P0.1 (or PIO0_1) is described in schematic: http://www.embeddedartists.com/sites/default/files/docs/schematics/LPCXpressoLPC1114revA.pdf
0 项奖励
回复

4,017 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by andrei.badila on Fri Sep 07 05:49:23 MST 2012

Quote: Zero
And did you enable vector catch and switch to ISP already?

See: http://support.code-red-tech.com/CodeRedWiki/DebugAccessChip



Sorry zero i don't found ISP pin( PIN 0.1). Please tell me wherein ISP PIN. I don't  speak very good English, please explain to me the steps to do:
"That is, GND the ISP pin, assert RST, then remove the GND to ISP pin. Once in the ISP bootloader, the target clock configuration is stable, and the debug pins are in their default state - you should be able to connect.
Note: The ISP pin is:
P0.1 - for LPC11xx and LPC13xx"
0 项奖励
回复

4,017 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Sep 07 04:29:15 MST 2012
And did you enable vector catch and switch to ISP already?

See: http://support.code-red-tech.com/CodeRedWiki/DebugAccessChip
0 项奖励
回复