Problem with lpc-link in debug

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with lpc-link in debug

718 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by achien98 on Fri Apr 02 00:37:25 MST 2010
after starting the "debug", the LPCXpresso IDE  trying to connect to the lpc-link board (LPC1114)through USB,  but it stopped at "Launching xxx(Debug):(96%)"  and shows LPCxpresso:Error: " Error launching Debug\xxx.axf    Remote communication error: No error. "   and hang,  unless I click the OK button in the Error message to stop the "debug"  process.

The LED shows "RED" on the target side of lpc-link board.

something wrong?   the windows xp control panel shows the USB driver for LPC-link debug probe v.1.1 looks ok.

Need help!
0 项奖励
回复
1 回复

708 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Connection on Sun Apr 04 22:47:05 MST 2010
Can you try following steps :
1. Go to tab window, select preference.
2. A dialog is opened, then expand tree LPCXpresso
3. Select Debug, check box "Initialize PC-link as HID..." in the window at right-hand side.
4. Make sure right MCU in the your target board ( by selecteion MCU)
5. Apply and OK.
6. Try again.

Best regards.
0 项奖励
回复