Problem with lpc-link in debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with lpc-link in debug

694件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by achien98 on Fri Apr 02 00:37:25 MST 2010
after starting the "debug", the LPCXpresso IDE  trying to connect to the lpc-link board (LPC1114)through USB,  but it stopped at "Launching xxx(Debug):(96%)"  and shows LPCxpresso:Error: " Error launching Debug\xxx.axf    Remote communication error: No error. "   and hang,  unless I click the OK button in the Error message to stop the "debug"  process.

The LED shows "RED" on the target side of lpc-link board.

something wrong?   the windows xp control panel shows the USB driver for LPC-link debug probe v.1.1 looks ok.

Need help!
0 件の賞賛
返信
1 返信

684件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Connection on Sun Apr 04 22:47:05 MST 2010
Can you try following steps :
1. Go to tab window, select preference.
2. A dialog is opened, then expand tree LPCXpresso
3. Select Debug, check box "Initialize PC-link as HID..." in the window at right-hand side.
4. Make sure right MCU in the your target board ( by selecteion MCU)
5. Apply and OK.
6. Try again.

Best regards.
0 件の賞賛
返信