Peripherals+ empty

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Peripherals+ empty

1,336件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tvink on Fri Dec 12 08:14:02 MST 2014
Hi,

I am debugging an LPC2294/01 and have paused execution in the debugger.
I press the Peripherals+ tab in the view thingie.  Nothing displays.
I can press Variables and see those.
I can press Breakpoints and see those.

But no peripheral registers. 

The project was created and built for the LPC2294/01.
I have linked the LP22xx.h header file so I can program the peripherals.

What am I missing.

Thanks
0 件の賞賛
返信
4 返答(返信)

1,317件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tvink on Mon Dec 15 07:19:28 MST 2014
Thanks for setting me straight. 

I was misinformed on an earlier posting where I asked " Would these two issues go away if I bought an LPCXpresso Version 2 evaluation board and used it as my debug pod?" and the supplied answer was yes.
0 件の賞賛
返信

1,317件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by whitecoe on Fri Dec 12 10:39:28 MST 2014

Quote: tvink

I have an LPC-Link2 probe on order.



That might have been a mistake given the part you are using - http://www.lpcware.com/content/faq/lpcxpresso/lpc-link2-support

You might want to go and order an LPC-Link1/LPCXpresso board instead…
0 件の賞賛
返信

1,317件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tvink on Fri Dec 12 08:51:40 MST 2014
Bummer!  Thanks,


I have an LPC-Link2 probe on order.
0 件の賞賛
返信

1,317件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Dec 12 08:29:10 MST 2014
I think from an earlier post you are using J-Link as your debug probe. The Peripheral view is not supported in J-Link.
0 件の賞賛
返信