Where is loader's output map file ??

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is loader's output map file ??

778件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Michael.Eaton on Fri Dec 12 09:24:13 MST 2014
Having apparent mem map problem attempting to use LPC4313 on Xpresso v7.5.  The program loads fine into an LPC4337 NGX demo board, but when processor selection is changed to LPC4313 to use on a different board, the debugger reports "no source available for 0x19e80c8c" - no physical memory exists at this loc.

I need to inspect the linker map file to find where it is trying to put the various code blocks.  What is filename for this file, and where is it?

Thank you,
Michael Eaton
0 件の賞賛
返信
1 返信

762件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Michael.Eaton on Fri Dec 12 10:24:25 MST 2014
Found it - no reply needed.
Thanks,
Mike
0 件の賞賛
返信