Object format by LPCXpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Object format by LPCXpresso IDE

671件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Thucydides on Tue Oct 19 02:24:18 MST 2010
Hello,
Today I got LPCXpresso1768 and its baseboard of Embedded Artists.
I tried some execution on the board it's quite nice I liked it.
By the way I have a question about object format generated by LPCXpresso IDE.
I think LPCXpresso is originally designed to download object using LPC-Link.
But I want to try to download using Flash Magic by NXP or J-Flash ARM by Segger.
So far I see there writing tools, they seem to only support .hex as object format.
So is it possible to generate .hex object not .axf by LPCXPresso?
I would be glad if someone give me information, since I'm really novice for it.
Thanks,
Thucydides
[B][/B]
0 件の賞賛
返信
1 返信

659件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Oct 19 02:35:50 MST 2010
A good place to look for information like this is the support knowledgebase:
http://lpcxpresso.code-red-tech.com/LPCXpresso/softwareknowledgebase

Your particular question is answered here:
http://support.code-red-tech.com/CodeRedWiki/OutputFormats
0 件の賞賛
返信