No compatible emulators available

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No compatible emulators available

2,187件の閲覧回数
thiazathasthake
Contributor I

Hi,

I installed the LPC platform (LPCXpresso v8.2.2_650) following the guide lines provided in the NxH2281 Getting started guide. But after setting up the hardware, and going through the program flash, it was popping, saying "No compatible emulators available". Please help me to rectify this problem.

Thanks

0 件の賞賛
返信
1 返信

1,827件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

You don't say what debug probe you are using or what host operating system. But if you are using an LPC-Link2, then in the first place see:

Booting LPC-Link2 

LPC-Link2 fails to enumerate with CMSIS-DAP firmware 

And if you are using the original LPC-Link, then look at:

https://community.nxp.com/message/630541 

If these don't help, then please provide more details of your setup and what exactly you have tried to get things working.

Regards,

LPCXpresso Support

0 件の賞賛
返信