No compatible emulators available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No compatible emulators available

2,185 Views
thiazathasthake
Contributor I

Hi,

I installed the LPC platform (LPCXpresso v8.2.2_650) following the guide lines provided in the NxH2281 Getting started guide. But after setting up the hardware, and going through the program flash, it was popping, saying "No compatible emulators available". Please help me to rectify this problem.

Thanks

0 Kudos
Reply
1 Reply

1,825 Views
lpcxpresso_supp
NXP Employee
NXP Employee

You don't say what debug probe you are using or what host operating system. But if you are using an LPC-Link2, then in the first place see:

Booting LPC-Link2 

LPC-Link2 fails to enumerate with CMSIS-DAP firmware 

And if you are using the original LPC-Link, then look at:

https://community.nxp.com/message/630541 

If these don't help, then please provide more details of your setup and what exactly you have tried to get things working.

Regards,

LPCXpresso Support

0 Kudos
Reply