Monitoring Stack Size

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Monitoring Stack Size

3,631件の閲覧回数
historysmistory
Contributor I

I am developing an application for the LPC4088 using the LPC-Link2 probe and I am looking for ways to monitor the size of the stack ideally in real time. Any suggestions?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,719件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信

2,719件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

There are a number of ways this might be done.

One idea is to capture the stack pointer from an interrupt routine such as systick. LPCXpresso IDE creates projects using a single stack model for exceptions - but take care that you monitor the intended stack.  Code like the example below could be used the capture the stack:

__STATIC_INLINE uint32_t __get_MSP(void)

{

  register uint32_t __regMainStackPointer     __ASM("msp");

  return(__regMainStackPointer);

}

Once the data has been captured, it could be saved into a global variable, then within LPCXpresso IDE this global variable could be monitored using SWO Datatrace.

Overview of Trace support in LPCXpresso IDE

Yours,

LPCXpresso-support

0 件の賞賛
返信