Modelling with eTrice and LPCXpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Modelling with eTrice and LPCXpresso

616 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by JungThom on Mon Dec 22 07:19:50 MST 2014
Hi all,

there is a new modelling tool called eTrice. It is completly open source and it can be installed directly into LPCXpresso. The tool is able to generate your complete C-Code out of a model.
The underlaying methodology is based on ROOM (Realtime Object Oriented Modelling).


http://de.wikipedia.org/wiki/Real_Time_Object_Oriented_Modeling

ROOM is very powerfull but relativly simple to use (other than UML).

It ist really simple to add it to your LPCXpresso 7 installation. Just install it from the update site

LPCXpresso:
Help->install new software

add the following update site

http://download.eclipse.org/etrice/updates/nightly/

Have fun.
Thomas
0 Kudos
Reply
0 Replies