Managed Linkerscript

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Managed Linkerscript

1,222件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MaSt on Thu Nov 14 04:21:13 MST 2013
Hi,
how do i force LPCXpresso 6.1.0 to update the managed linkerscript? I use it for managing a LPC4337 Project, but it does not update the used linkerscript. I deleted the linkerscript, afterwards LPCXpresso complained about missing it. How do i generate a new one?

Thanks.
0 件の賞賛
返信
3 返答(返信)

1,213件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Nov 14 05:06:23 MST 2013
Are you sure you are using a Managed Linker script? Clean and rebuild will recreate linker script, if your project is setup that way. You can check this on the MCU Linker/Target settings - the "Manage linker script" option should be checked.

0 件の賞賛
返信

1,213件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MaSt on Thu Nov 14 04:57:12 MST 2013
This was the first thing i did (several times before posting here). Unfortunately this did not solve the problem.
0 件の賞賛
返信

1,213件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Nov 14 04:39:49 MST 2013
Clean and then rebuild
0 件の賞賛
返信