.axf file deleted

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

.axf file deleted

676 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by userrr on Tue Sep 17 01:20:59 MST 2013
I want to create a .bin file from lpcxpresso and i followed this tutorial http://www.microbuilder.eu/blog/10-01-12/Creating_Valid_LPC1343_Binaries_in_LPCXpresso.aspx
The problem is that when i build the project, the name.axf file is deleted automatically  the error regarding RamLoc32 overflowed takes place.

PS: I tried to build the project without creating the .bin file and the same thing happened.

Thank you!
0 Kudos
Reply
1 Reply

637 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Tue Sep 17 01:43:25 MST 2013
The .axf file is not being deleted - it is not being created!

You must fix your linker error first. The error means that you application is too big for the RamLoc32 memory region. Use forum search to find why this might have happened
0 Kudos
Reply