Looking for a free compiler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Looking for a free compiler

1,389件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Senso on Wed Nov 17 16:23:05 MST 2010
Goodnight to everybody, can someone help me about how to get the free arm-gcc compiler compiling code for the LPCXpresso1768 board.
Thanks in advance.
0 件の賞賛
返信
5 返答(返信)

1,330件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Thu Nov 18 17:05:39 MST 2010
The [SIZE=4][B]compiler[/B][/SIZE] ([COLOR=#000000]Enter your favorite in this line_____________[/COLOR]) has no limit.

The [SIZE=4][B]debugger[/B][/SIZE] ([COLOR=#000000]Combination of hardware and software[/COLOR]) has the 128k limit.

If the communication protocol of the LPC-Link was free and open there is no such limit. So it is not free nor open. :D

Oh! [COLOR=#000000]You can also purchase a license to remove the limit or use another product.[/COLOR]
0 件の賞賛
返信

1,330件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Senso on Thu Nov 18 16:43:21 MST 2010
And it keeps doing the upload to the board even if the code exceeds the 128Kb limit?
Thanks for the response.
0 件の賞賛
返信

1,330件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Nov 18 10:36:48 MST 2010
The *compiler* has no limit.
The *debugger* has the 128k limit.
0 件の賞賛
返信

1,330件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by thinkchip on Thu Nov 18 10:24:33 MST 2010
but, there is no limit 128k to program memory flash??
0 件の賞賛
返信

1,330件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Nov 18 00:58:00 MST 2010
The LPCXpresso IDE is free and uses gcc. Read the Getting started to see how to use it:
http://ics.nxp.com/support/documents/microcontrollers/pdf/lpcxpresso.getting.started.pdf
0 件の賞賛
返信