SVN integration in LPCXpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SVN integration in LPCXpresso

956 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kralux on Wed Nov 17 15:07:31 MST 2010
Is there anyway to have SVN handled from within the LPCXpresso IDE?

Good IDEs like IntelliJ IDEA do integrate most common source control versioning protocols like CVS, SVN, ...

Thank you.

Original Attachment has been moved to: 1100840_LPC1778-PLL-Calculator.zip

0 Kudos
Reply
2 Replies

829 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kralux on Thu Nov 18 11:35:08 MST 2010
:) That is great!
Thanks a lot.
0 Kudos
Reply

829 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Nov 18 00:56:18 MST 2010
LPCXPresso is based on Eclipse, for which there are (literally) hundreds of enhancements (plugins) available, including two for integration with Subversion. Details on integration with some version control systems can be found on our support system, here:
http://support.code-red-tech.com/CodeRedWiki/VersionControl

If it helps, internally, we use Subclipse.
0 Kudos
Reply