Launching project never finishes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Launching project never finishes

2,251 Views
alexbrz
Contributor I

Hello everyone!

I have worked on a project for a couple years, using LPC1115 and LPCxpresso IDE v7.7.2 and it always worked fine. This week I have two new boards done with some little modifications, and have only been able to launch my program in one of them. For the other one, the launching process stuck at 97% and never finish.

I'm thinking it's probably a problem with the microcontroller in that board, once the connections are ok.

Anyone had a similar problem and can help me? Thanks in advance!

Labels (1)
2 Replies

2,054 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Hi,

could you please attach all the logs?

  • IDE .log file in <your workspace>/.metadata folder
  • Build console log
  • gdb traces and other console logs
  • Debug Messages console log

Regards,

MCUXpresso IDE support team

2,054 Views
alexbrz
Contributor I

Hi, thanks for the reply.

It turned out to be really a hardware problem, which we solved by replacing the microcontroller.

Though we don't know wether it was a part failure or welding problem, once it is a very sensitive but reliable component.

0 Kudos
Reply