LPCxpresso 1114 - problem with examples

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCxpresso 1114 - problem with examples

1,832件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by RWM on Wed May 05 15:02:52 MST 2010
Hi, I have problem with LPCXpresso1114_systick_twinkle example. When I try to debug it, error is reported:
Target reports license restriction
License type is License type: FULL
Debug limit: 128k

When I tried second time, following error was reported:
Target reported errors:
Reason:
License restriction: Flash image too large for this license

I think this example is smaller than 128k, LPC1114 has only 32k of Flash. LPCXpresso1114_blinky example works. I use LPCXpresso 3.3.4. Any idea?
0 件の賞賛
返信
8 返答(返信)

1,817件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lki99 on Sun May 16 15:30:33 MST 2010
New 'beta' version of  LPCxpresso solves my problem too. Thanks to Code Red Support.
0 件の賞賛
返信

1,817件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sun May 16 11:58:28 MST 2010
Please contact Code Red Support via this page:
http://www.code-red-tech.com/support.php
0 件の賞賛
返信

1,817件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lki99 on Sun May 16 05:46:52 MST 2010
Hello, CodeRedSupport

In "Display License Type" menu message is:
License type: FULL
Debug Limit 128k


When I try to debug Example "LPCXpresso1343_consoleprint", I get error message:
Target reported errors
License restriction: Flash image too large for this license.


When I try to use command line flash loader, I have this output:

crt_emu_lpc11_13_nxp.exe -wire=winusb -flash-load=c:\1.bin -pLPC1343
Ni: LPCXpresso Debug Driver v2.0 (Apr  8 2010 14:57:58)
Nc: Looked for chip XML file in C:/nxp/lpcxpresso_3.3/bin/LPC1343.xml
Nc: Looked for vendor directory XML file in C:/nxp/lpcxpresso_3.3/bin/nxp_directory.xml
Nc: Found generic directory XML file in C:/nxp/lpcxpresso_3.3/bin/crt_directory.xml

Nc: NXP: LPC1343  Part ID: 3D00002B
Wt: License check failure (CheckLicense)
Cr:f Restricted - unregistered license, download limit of 8K
Et:53: License does not permit flash operations from command line

Where is the problem?
0 件の賞賛
返信

1,817件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sun May 16 01:48:50 MST 2010
The beta is not generally available. It was a special release specifically for RWM.

Can you explain exactly what your problem is, as it is likely that it is a different problem to that reported by RWM.
0 件の賞賛
返信

1,817件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lki99 on Sat May 15 14:32:26 MST 2010

Quote: RWM
Problem solved by Code Red Support - new (beta) version of LPCxpresso.



And where is this new beta version - I have the same problem with my    LPCxpresso 1343?
0 件の賞賛
返信

1,817件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by RWM on Wed May 12 04:57:34 MST 2010
Problem solved by Code Red Support - new (beta) version of LPCxpresso.
0 件の賞賛
返信

1,817件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu May 06 09:59:50 MST 2010
RWM,

It might be faster if you can contact Code Red support through our  support web page.
http://www.code-red-tech.com/support.php

We'd like to send a license diagnostic for you to run. It produces one  or two output files you'll need to return. These files do not contain  personal information if you're concerned.

Regards,

CodeRedSupport
0 件の賞賛
返信

1,817件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Wed May 05 18:21:13 MST 2010

Quote: RWM
Hi, I have problem with LPCXpresso1114_systick_twinkle example. When I try to debug it, error is reported:
Target reports license restriction
License type is License type: FULL
Debug limit: 128k

When I tried second time, following error was reported:
Target reported errors:
Reason:
License restriction: Flash image too large for this license

I think this example is smaller than 128k, LPC1114 has only 32k of Flash. LPCXpresso1114_blinky example works. I use LPCXpresso 3.3.4. Any idea?




Not your fault, is a  manufacturing fault (a feature, say some):


[LIST]
[*][B]Version 3.3 license restriction, image size?[/B]
[*][B]Invalid Activation Code[/B]
[*][B]v3.3.4 error message, License restriction:[/B]
[*]...
[/LIST]
0 件の賞賛
返信