LPCXpresso with LPC824 - why it is not possible to create a CMSIS project?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso with LPC824 - why it is not possible to create a CMSIS project?

1,221件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ledi007 on Wed Feb 17 02:42:03 MST 2016
Hi guys,

i want to create a new project with a LPC824 controller in a new workspace with LPCXpressoV8.0.0.
But, i dont get a window, where i can select the import of a CMSIS core library. (look @ image cmsis1)

If i choose another controller like the LPC1114, it is possible (look @ image cmsis2) to import the CMSIS core library. :O

Now, i am confused! Why is that :quest:
0 件の賞賛
返信
2 返答(返信)

1,162件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ledi007 on Wed Feb 17 03:31:09 MST 2016
ok, i understood.

But why?
Should CMSIS not be the standard?

Is nxp cooking it´s own soup with lpcopen?

Where is the sence of a standard, if each vendor make it´s own libraries? :~
Maybe, it should not be, to give a software developer an easy way to change the manufacturer of a controller?
0 件の賞賛
返信

1,162件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Feb 17 03:13:37 MST 2016

Quote: ledi007
If i choose another controller like the LPC1114, it is possible (look @ image cmsis2) to import the CMSIS core library. :O

Now, i am confused! Why is that :quest:



Because LPC11xx is a very old family (7 years), which started with CMSIS support  ;-)

Newer families are using LPCOpen, so there's no CMSIS available...
0 件の賞賛
返信