LPCXpresso with LPC824 - why it is not possible to create a CMSIS project?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso with LPC824 - why it is not possible to create a CMSIS project?

1,192 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ledi007 on Wed Feb 17 02:42:03 MST 2016
Hi guys,

i want to create a new project with a LPC824 controller in a new workspace with LPCXpressoV8.0.0.
But, i dont get a window, where i can select the import of a CMSIS core library. (look @ image cmsis1)

If i choose another controller like the LPC1114, it is possible (look @ image cmsis2) to import the CMSIS core library. :O

Now, i am confused! Why is that :quest:
0 项奖励
回复
2 回复数

1,133 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ledi007 on Wed Feb 17 03:31:09 MST 2016
ok, i understood.

But why?
Should CMSIS not be the standard?

Is nxp cooking it´s own soup with lpcopen?

Where is the sence of a standard, if each vendor make it´s own libraries? :~
Maybe, it should not be, to give a software developer an easy way to change the manufacturer of a controller?
0 项奖励
回复

1,133 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Wed Feb 17 03:13:37 MST 2016

Quote: ledi007
If i choose another controller like the LPC1114, it is possible (look @ image cmsis2) to import the CMSIS core library. :O

Now, i am confused! Why is that :quest:



Because LPC11xx is a very old family (7 years), which started with CMSIS support  ;-)

Newer families are using LPCOpen, so there's no CMSIS available...
0 项奖励
回复