LPCXpresso jtag

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso jtag

1,368 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aferrari on Mon Jul 27 07:55:59 MST 2015
Hello everyone,

I'd like to use LPCXpresso with lpc4078 ARM Cortex-M4 MCU.

Do you know what kind/model of jtags are supported by LPCXpresso?

Thanks in advance.

Alberto Ferrari
0 Kudos
Reply
5 Replies

1,327 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aferrari on Mon Jul 27 09:35:29 MST 2015
Thanks again for your kindness.

Regards

Alberto Ferrari
0 Kudos
Reply

1,327 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Jul 27 08:53:00 MST 2015
No, Windows XP is not supported. v7.9.0 now introduces support for WIndows 10...

The last version of LPCXpresso that we tested on XP was 7.0.2.
0 Kudos
Reply

1,327 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aferrari on Mon Jul 27 08:44:58 MST 2015
Dear Support and miccio,

thank you very much for the reply.

Yes I was talking about the Debug Probe. Thanks for the hints.

Another question if you can answer in this post....

I've downloaded the latest LPCXpresso release (7.9.0_455).
It was written that LPCXpresso may continue to work on Windows XP, even if WXP is no longer supported, but when I started the installation the following error arises:

"This program does not support the version of Windows your computer is running"

Could you tell me the latest LPCXpresso version that I can use with Windows XP?

Thanks a lot

Alberto Ferrari
0 Kudos
Reply

1,327 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by miccio on Mon Jul 27 08:12:31 MST 2015
ciao Alberto,

this board here http://www.nxp.com/demoboard/OM13038.html comes with a built in debugged which is allegedly compatible with LPCXpresso.
If you would rather have an external debugger, here's the LPC-Link 2 http://www.nxp.com/demoboard/OM13054.html :)
0 Kudos
Reply

1,327 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Jul 27 08:05:17 MST 2015
I assume that you are asking what types of Debug Probe is supported by LPCXpresso?

Basically, you need something that supports CMSIS-DAP, such as LPC-Link2, Ulink-ME, Ulink-Pro etc.

LPCXpresso also supports some older style adapters, including LPC-Link and Red Probe+.

0 Kudos
Reply