LPCXpresso Using ISP Uart Flash Program

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso Using ISP Uart Flash Program

2,074 Views
mrcbis
Contributor I

Hello,

I am just starting using LPCXpresso IDE under Ubuntu 16.04LTS. I wonder if there is any way to program OnChip flash memory using ISP Uart BootLoader mode of the device. I am able to communicate with the chip using lpctools but I wonder if there is some way to integrate the flash programming phase inside the LPCXpresso IDE. I have a custom board and I have no jtag connection available. The only way to program the flash memory is using a Uart cable to download image to the device (using an USB -> Uart adapter that is working with lpctools).

Regards

Marco Bisio

0 Kudos
Reply
1 Reply

1,623 Views
converse
Senior Contributor V

Nothing in the ide, but try mxli: mxli - Marc's exquisite LPC ISP tool 

0 Kudos
Reply