LPCXpresso 'Manage linker script' feature / bug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso 'Manage linker script' feature / bug

1,476件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Apr 27 10:28:16 MST 2012
Every time I copy a (cleaned) project and rename it, linker script file names (*.ld) are not updated :mad:

My workaround is to disable 'Manage linker script', clean my project and reenable 'Manage linker script' again :rolleyes:

Now new linker script files are generated and I can delete the old ones :)

Is this a feature, a bug or am I just too dump to find an 'Automatic linker script file Update' button?
0 件の賞賛
返信
5 返答(返信)

1,429件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Sep 20 05:44:22 MST 2012
Yes, still on the list.

Regards,
CodeRedSupport
0 件の賞賛
返信

1,429件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Sep 20 05:20:42 MST 2012

Quote: CodeRedSupport
...it is on the list of things to be looked at for a future release...
CodeRedSupport



Just tested V4.3.0 without success :(

Is this issue still on the list :confused:
0 件の賞賛
返信

1,429件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Apr 27 13:15:45 MST 2012

Quote: CodeRedSupport
...it is on the list of things to be looked at for a future release.




Good to know, thanks :)
0 件の賞賛
返信

1,429件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Apr 27 12:54:33 MST 2012
Zero - you're right. I've hit this caching issue myself and it is on the list of things to be looked at for a future release. Your workaround is the simplest one that I am aware of.

PS - Hello Larry - it's been a while!

Regards,
CodeRedSupport
0 件の賞賛
返信

1,429件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larryvc on Fri Apr 27 11:01:30 MST 2012
"dumb" not "dump".  You can be the former, you can take the latter. :rolleyes:

I would say it is a bug or an undesirable feature. :)  I'm back...
0 件の賞賛
返信