LPCXpresso IDE v4.3.0 OSX Activation problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso IDE v4.3.0 OSX Activation problem

1,952 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by yoko on Thu Sep 27 12:23:41 MST 2012
Hi,

     I just install the new LPCXpresso IDE v4.3.0 OSX version.  It seems to be the Redsuite version that was uploaded.  I am unable to activate LPCXpresso license.  How can I make it work ? Thanks

Hoan
0 Kudos
Reply
10 Replies

1,939 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Sun Oct 28 20:26:35 MST 2012
use the archiver to decompress the .tar.gz files into a .app, and then run it. If you do this through the finder, it should 'just work'.
0 Kudos
Reply

1,939 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wa7iut on Sun Oct 28 13:02:26 MST 2012
I downloaded Installer_LPCXpresso_4.3.0_1033_MacOS-X.tar_.gz and I get the error "There is no application set to open the document "Installer.....".   So how do I get this to install on my iMac?  I'm running OS X version 10.8.2
0 Kudos
Reply

1,939 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by angelpozico on Mon Oct 01 02:15:21 MST 2012

Quote: CodeRedSupport
angelpozico,

We would like to discuss the problem you are having activating on Windows 7 directly. Please can you contact us via the "Email the support team" link at:

http://www.code-red-tech.com/support.php

quoting this forum thread.

Regards,
CodeRedSupport



Hi,

I just email to code_red product support

Best Regards

Angel
0 Kudos
Reply

1,939 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Oct 01 01:35:45 MST 2012
angelpozico,

We would like to discuss the problem you are having activating on Windows 7 directly. Please can you contact us via the "Email the support team" link at:

http://www.code-red-tech.com/support.php

quoting this forum thread.

Regards,
CodeRedSupport
0 Kudos
Reply

1,938 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by angelpozico on Sun Sep 30 08:28:14 MST 2012

Quote: CodeRedSupport
Please zip up and post your log file:
<workspace>/.metadata/.log



Hi, I hope I uploaded it correctly

[ATTACH]849[/ATTACH]


thanks
0 Kudos
Reply

1,938 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sat Sep 29 09:57:47 MST 2012
Please zip up and post your log file:
<workspace>/.metadata/.log
0 Kudos
Reply

1,938 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by angelpozico on Sat Sep 29 08:52:49 MST 2012

Quote: CodeRedSupport
Please try activating again (even though you have done it before):
1. Create a new Serial number and Activate
2.When you get the serial number, Enter Activation code

If this does not work, then please provide the exact error message that you see and also the actual OS (including version) that you are running.

Regards,
CodeRedSupport




Hi, thanks for your quick response

once I create serial number is written:

string index out of range -11
unable to store serial number
string index out of range -11

then, when I am going to enter the activation code appear:

no license to activate

I have a wondows 7, version 6.1 ( build 760 1: service Pack 1)

Thanks!

best regards

Angel
0 Kudos
Reply

1,938 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sat Sep 29 06:52:26 MST 2012
Please try activating again (even though you have done it before):
1. Create a new Serial number and Activate
2.When you get the serial number, Enter Activation code

If this does not work, then please provide the exact error message that you see and also the actual OS (including version) that you are running.

Regards,
CodeRedSupport
0 Kudos
Reply

1,938 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by angelpozico on Sat Sep 29 02:31:40 MST 2012
Hi,

I've just  installed LCP Xpresso, but I am unable to activate it

What do I have to do? since after doing everything is required (create serial number and activate and after that, enter activation code)   there is a message saying something like:

there is not license to activate

Many thanks!

Angel
0 Kudos
Reply

1,938 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Sep 27 13:29:29 MST 2012
The correct LPCXpresso installer for OSX has now been posted. Please download this new version.
0 Kudos
Reply