LPCXpresso Free code space limitation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso Free code space limitation

1,392 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giusloq on Thu May 14 15:20:01 MST 2015
I know Free edition restricts programming and debugging of applicati on greater Ethan 256.
It's not clear to me where si exactly the limitation.


For exampla: LPCXpresso Free Edition and LPCLink devboard. If I'll be able to configure standard Eckipse or Code::Blocks and LPCLink as a standard GDB server. Will the restricion disappear? In this case the IDE isn't LPCXpresso so I could immagine the limitation doesn't apply, but I use the debugger driver that comes with LPCXpresso so I don't know.

0 Kudos
Reply
4 Replies

1,356 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giusloq on Fri May 15 02:14:46 MST 2015

Quote:
This may help:
http://www.lpcware.com/content/forum/lpcxpresso-segger-j-link#comment-1145323


Even in that thread, it's not clear if the memory size restriction of LPCXpresso Free Edition would be present with J-Link probe or not.
0 Kudos
Reply

1,356 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Fri May 15 01:48:52 MST 2015
This may help:
http://www.lpcware.com/content/forum/lpcxpresso-segger-j-link#comment-1145323
0 Kudos
Reply

1,356 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by giusloq on Fri May 15 00:01:36 MST 2015
I understand. So put the question in the opposite way.

If I buy a J-Link debugger/programmer probe from Segger, could I use it with LPCXpresso Free Edition to program and debug applications without any restrictions on code size?
0 Kudos
Reply

1,356 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu May 14 23:10:59 MST 2015
The limitation is implemented in the debugger. You can generate an application of any size, but the debugger will not debug an image large than 256k
0 Kudos
Reply