LPCXpresso 7.7.2 - Modifying PIN value or Direction Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso 7.7.2 - Modifying PIN value or Direction Error

861 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Carl-CircuitWorx on Mon Apr 20 04:58:19 MST 2015
Hi,

Using the latest LPCXpresso, when I manually change the value of a PIN via the memory tab opened by the Peripherals+ view I get the following error :

33: Unknown register in register modify GPIO-PORT.PIN-0-.PORT12

Same error when trying to modify a direction value via the DIR register

Using an LPC1549, debugger is paused.

0 项奖励
回复
2 回复数

849 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Carl-CircuitWorx on Mon Apr 20 09:27:03 MST 2015
Glad I can help :)

Carl.
0 项奖励
回复

849 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Apr 20 08:21:27 MST 2015
We have reproduced the problem and are investigating.

Thanks for the problem report and sorry for the inconvenience.
0 项奖励
回复