LPC1769 dev board choice

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1769 dev board choice

982 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alpha on Wed Jun 06 02:20:11 MST 2012
Can I know what is the difference between these two boards?

http://sg.mouser.com/ProductDetail/Embedded-Artists/EA-XPR-003/?qs=S92LKl1JvFyxqKp2Q1rskQ%3d%3d

http://sg.element14.com/nxp/om13000/board-lpcxpresso-lpc1769/dp/1825878

Does both of them have the same LPC-link?

Thanks
0 项奖励
回复
3 回复数

969 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alpha on Wed Jun 06 03:53:08 MST 2012
Thanks for the clarification. I was quite confused with the 2 boards having different name and ID.
0 项奖励
回复

969 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Jun 06 02:31:10 MST 2012

Quote: alpha
Can I know what is the difference between these two boards?

http://sg.mouser.com/ProductDetail/Embedded-Artists/EA-XPR-003/?qs=S92LKl1JvFyxqKp2Q1rskQ%3d%3d

http://sg.element14.com/nxp/om13000/board-lpcxpresso-lpc1769/dp/1825878

Does both of them have the same LPC-link?



Even worse, it's the same board :eek:

Since EA and NXP are selling this board there are sometimes different order numbers (and sometimes even different prices :rolleyes:).

But they are all LPCXpresso1769 (since LPCXpresso1768 is sold out long time ago) :)
0 项奖励
回复

969 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by frame on Wed Jun 06 02:30:13 MST 2012
I believe it's the same board (EA LPCXpresso LPC1769), only from different distributors.
0 项奖励
回复