LPC1769 dev board choice

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1769 dev board choice

980 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alpha on Wed Jun 06 02:20:11 MST 2012
Can I know what is the difference between these two boards?

http://sg.mouser.com/ProductDetail/Embedded-Artists/EA-XPR-003/?qs=S92LKl1JvFyxqKp2Q1rskQ%3d%3d

http://sg.element14.com/nxp/om13000/board-lpcxpresso-lpc1769/dp/1825878

Does both of them have the same LPC-link?

Thanks
0 Kudos
Reply
3 Replies

967 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alpha on Wed Jun 06 03:53:08 MST 2012
Thanks for the clarification. I was quite confused with the 2 boards having different name and ID.
0 Kudos
Reply

967 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Jun 06 02:31:10 MST 2012

Quote: alpha
Can I know what is the difference between these two boards?

http://sg.mouser.com/ProductDetail/Embedded-Artists/EA-XPR-003/?qs=S92LKl1JvFyxqKp2Q1rskQ%3d%3d

http://sg.element14.com/nxp/om13000/board-lpcxpresso-lpc1769/dp/1825878

Does both of them have the same LPC-link?



Even worse, it's the same board :eek:

Since EA and NXP are selling this board there are sometimes different order numbers (and sometimes even different prices :rolleyes:).

But they are all LPCXpresso1769 (since LPCXpresso1768 is sold out long time ago) :)
0 Kudos
Reply

967 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by frame on Wed Jun 06 02:30:13 MST 2012
I believe it's the same board (EA LPCXpresso LPC1769), only from different distributors.
0 Kudos
Reply