LPC1768 using RMII

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1768 using RMII

1,536件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Jonno on Wed Jun 03 03:36:13 MST 2015
Hi,

I am using a LPC1768 connected to a KSZ8873RLLI 3 port ethernet switch on a custom board. I am using the RMII interface to communicate between the LPC1768 and the KSZ8873. I am struggling to know where to start with the initialisation of the RMII interface on the LPC1768. I have found lpc17xx_emac (in the sample programs that come with LPCXpresso) but am not sure if this is appropriate for these devices, as it refers to TI ethernet chip DP83848C, and am not even sure it uses RMII.

Any help would be appreciated.
タグ(2)
0 件の賞賛
返信
1 返信

1,422件の閲覧回数
bruce_chen
Contributor I

Hello:

     Are you successed useing for RMII with switch chip?

0 件の賞賛
返信