LPC1768 using RMII

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1768 using RMII

1,621 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Jonno on Wed Jun 03 03:36:13 MST 2015
Hi,

I am using a LPC1768 connected to a KSZ8873RLLI 3 port ethernet switch on a custom board. I am using the RMII interface to communicate between the LPC1768 and the KSZ8873. I am struggling to know where to start with the initialisation of the RMII interface on the LPC1768. I have found lpc17xx_emac (in the sample programs that come with LPCXpresso) but am not sure if this is appropriate for these devices, as it refers to TI ethernet chip DP83848C, and am not even sure it uses RMII.

Any help would be appreciated.
0 Kudos
Reply
1 Reply

1,507 Views
bruce_chen
Contributor I

Hello:

     Are you successed useing for RMII with switch chip?

0 Kudos
Reply