LPC1756 Erase error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1756 Erase error

2,164件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by szempy on Fri Mar 25 07:02:11 MST 2016
When i try to erase my LPC1756 processor i get this error :

Ed:04: Failed to erase flash: Em(12). System rejected access at location 0xFFFFFFFF - verify Population of memory and peripherals

Ni: LPCXpresso RedlinkMulti Driver v8.1 (Mar 11 2016 13:34:34 - crt_emu_cm_redlink.exe build 672)
Pc: (  0) Reading remote configuration
Nc: Found chip XML file in D:/Melo/Tachosafe 4/FW LPC/Bootloader/Release/LPC1756.xml

Pc: (  5) Remote configuration complete
Nc: Probe Firmware: LPC-Link Probe v1.3 (NXP - LPC-Link)
Nc: Serial Number:  HID64HS12
Nc: VID:PID:  1FC9:0007
Nc: USB Path: 
Pc: ( 30) Emulator Connected
Pc: ( 40) Debug Halt
Pc: ( 50) CPU ID
Nc: Emu(0): Connected&Reset. DpID: 2BA01477. CpuID: 410FC230. Info: <None>
Nc: Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
Nc: inspected v.2 On-chip Flash Memory C:\nxp\LPCXpresso_8.1.4_606\lpcxpresso\bin\Flash\LPC175x_6x_256.cfx
Nc: image 'LPC175x_6x (256K) Feb 16 2016 09:18:54'
Nc: NXP: LPC1756  Part ID: 0x00000000
Pc: ( 65) Chip Setup Complete
Nt: Connected: was_reset=false. was_stopped=true
Cr:v LPCXpresso Free License - Download limit is 256K
Pc: ( 70) License Check Complete
Ed:04: Failed to erase flash: Em(12). System rejected access at location 0xFFFFFFFF - verify Population of memory and peripherals
Pc: (100) Target Connection Failed
0 件の賞賛
返信
7 返答(返信)

2,123件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信

2,123件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by szempy on Thu Mar 31 00:37:38 MST 2016
Thank you for your answer i know that you would replay this link, because i already searched the forum but that didn't help.
Now i am getting this error message :
Ni: LPCXpresso RedlinkMulti Driver v8.1 (Mar 11 2016 13:34:34 - crt_emu_cm_redlink.exe build 672)
Pc: (  0) Reading remote configuration
Nc: Found chip XML file in D:/Melo/Tachosafe 4/FW LPC/Bootloader/Release/LPC1756.xml

Pc: (  5) Remote configuration complete
Ed:02: Failed on connect: Ee(36). Could not connect to core.
Et:31: No connection to emulator device
Pc: (100) Target Connection Failed


I have replaced my LPC-Link with another one and that one is working, so it is most like that the LPC-LINK got damaged somehow.
0 件の賞賛
返信

2,123件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Mar 30 11:58:01 MST 2016

Actually, your code can destabilize the part if, for example, the PLL Current Controlled Oscillator setting is out of range. If memory serves, there may have been an errata on the Fcco frequency range in the user manual. In any case, before digging further, read this FAQ.

Regaining debug access to target MCU

Thanks and regards,
LPCXpresso Support
0 件の賞賛
返信

2,123件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Wed Mar 30 01:52:58 MST 2016
That doesn't mean anything.
But given you have provided no information on what problems you are experiencing, it is impossible to offer any other advice. Good luck.
0 件の賞賛
返信

2,123件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by szempy on Wed Mar 30 01:45:45 MST 2016
The power is ok, as i wrote i can program it with flash magic but i can't with LP-Link.
0 件の賞賛
返信

2,123件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Wed Mar 30 01:18:27 MST 2016
Check your power. It is highly unlikely (impossible?) that your code damaged your chip.
0 件の賞賛
返信

2,123件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by szempy on Tue Mar 29 23:48:02 MST 2016
I could erase it with Flash Magic over ISP and program it, but it is behaving strange, maybe the software damaged somehow the processor ?
0 件の賞賛
返信