LPC1343 USB CDC Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1343 USB CDC Problem

1,007 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by julhio on Mon Jan 31 20:33:04 MST 2011
Hello.
I have a LPC1343 board and I can't work with LPC1343 Virtual Serial Port. I have programed the chip with USB CDC example, but when I connect the board on pc, this doesn't install de driver. I tryed to put the driver manually, but doesn't work too. :(
I have windows 7 x64.
Do you know any idea what I need to do ? :confused:

Best Regards,
Julhio.
0 Kudos
Reply
2 Replies

933 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ktownsend on Tue Feb 01 01:37:30 MST 2011
Some more information would be helpful.  I'm assuming if you're posting on the LPCXpresso forum that you are using the LPC1343 LPCXpresso board, though perhaps I'm mistaken.  If not, you'll need to indicate which board you are using.

As well ... you make no indication of which 'USB CDC firmware' you are using.  Where did the example come from?
0 Kudos
Reply

933 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Jan 31 20:40:01 MST 2011
Do you know that you need an additional USB-connector (or additional Base Board) ?

This Example is not working with LPC-Link USB-connector.

See http://knowledgebase.nxp.com/showthread.php?t=742

Win7 64bit driver see http://knowledgebase.nxp.com/showthread.php?t=1463
0 Kudos
Reply