LPC1227 PWM Output Invert

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1227 PWM Output Invert

1,315件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by spongehead on Tue Feb 26 02:15:56 MST 2013
I am running with an LPC1227 module.  I have 32-bit Timer 0 (CT32B0) configured for PWM.  Per the "PWM Rules" section of Users Manual,
it indicates that the generated pulse will be LOW for whatever the MR0 {in my case) is set for and HIGH to the end of the period (MR3 in my case).

Does anyone know a way to "invert" this pulse behavior, such that the MR0
output is "HIGH" till MR0 count and then will go "LOW" for remainder of the
period.  Don't want to add inverters on MR0-2 outputs if it can be done by some internal register setting that I am unaware of. 

Any info appreciated!
0 件の賞賛
返信
3 返答(返信)

1,262件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Feb 26 03:08:00 MST 2013
EMR :eek: usage is perhaps more clearly shown in #3 of http://knowledgebase.nxp.com/showthread.php?t=2785 :)
0 件の賞賛
返信

1,262件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by spongehead on Tue Feb 26 02:32:56 MST 2013
Thanks Zero... No I missed that thread.
Will check through your reply.
0 件の賞賛
返信

1,262件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Feb 26 02:23:27 MST 2013

Quote: spongehead
Any info appreciated!



Did you already read : http://knowledgebase.nxp.com/showthread.php?t=3724 :confused:
0 件の賞賛
返信