LPC1100 FFT Function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1100 FFT Function

821 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IanMorris on Thu Jun 24 15:25:01 MST 2010
The attached zip file contains an implementation of a 256-point FFT function for the Cortex-M0 family of products (LPC1100 devices) along with example projects for the Keil, IAR and CodeRed Software Development platforms.

The original implementation was kindly supplied by Chris Guarneri of NXP. The FFT function is provided as a prebuilt library file. The source for the FFT function is not supplied as it is based upon code that is only available from NXP under NDA.

Hopefully this will be of use to someone....
0 Kudos
Reply
0 Replies