LPC1100 FFT Function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1100 FFT Function

827件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IanMorris on Thu Jun 24 15:25:01 MST 2010
The attached zip file contains an implementation of a 256-point FFT function for the Cortex-M0 family of products (LPC1100 devices) along with example projects for the Keil, IAR and CodeRed Software Development platforms.

The original implementation was kindly supplied by Chris Guarneri of NXP. The FFT function is provided as a prebuilt library file. The source for the FFT function is not supplied as it is based upon code that is only available from NXP under NDA.

Hopefully this will be of use to someone....
0 件の賞賛
返信
0 返答(返信)