LPC link not getting connected

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC link not getting connected

758件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mary Cilna on Wed Jul 22 23:48:24 MST 2015
hi,
i updated my IDE to the latest version LPCXpresso v7.8.0_426. i imported my old project to the new ide and tried to program but  the LPC link is not getting conected . it just shows only progress information bar and unable to cancel it. the LPC link 2's led LED1 goes on blinking.

is it neccesary to rebuild the project as i imported it to updated  IDE?

need help.
regards
Cilna
0 件の賞賛
返信
2 返答(返信)

741件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mtesmer on Sat Jul 25 01:23:42 MST 2015
Hi,

I had a very similar problem and indeed all my trouble was related to the outdated UCOM driver for LPC-Link2.

Regards,
0 件の賞賛
返信

742件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Jul 23 00:25:21 MST 2015
It's unclear whether you are using the original LPC-Link or an LPC-Link2.

First of all, if you are using LPC-Link2, please check out the following FAQ:
https://www.lpcware.com/content/faq/lpcxpresso/lpc-link2-failing-enumerate-cmsis-dap-firmware

If that doesn't help please try going through the appropriate FAQ for the probe you are using below, in particular the troubleshooting sections.

https://www.lpcware.com/content/faq/lpcxpresso/booting-lpc-link
https://www.lpcware.com/content/faq/lpcxpresso/booting-lpc-link2

If you are still having problems, please confirm which probe you are using and provide details of what you see when working your way through the above FAQs,  together with what OS you are using.

Regards,
LPCXpresso Support
0 件の賞賛
返信