LPC Link, flash command line

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC Link, flash command line

1,735 次查看
rianzu
Contributor II

I have a LPC-Link that I'd like to use as command line programmer (Windows).

After IDE (LPC Xpresso) it initialize the boards, programming can be done by using a command line

C:\nxp\LPCXpresso_8.0.0_526\lpcxpresso\bin\crt_emu_cm3_gen -flash-load-exec "test_project/Release/test_project.axf" -g -2 -vendor=NXP -pLPC824 -wire=hid -s3000 -flash-driver=LPC800_32.cfx -x D:/test_project/Release

Now the question is how do I initialize the board like LPC Xpresso does?

Above line works until I unplug the USB from the board.

This is very convenient for production programming, so don't need IDE anymore.

Also, how can I provide the license in command line (a batch file probably) since I may use a computer that doesn't have a IDE installed.

Thanks in advance,

0 项奖励
回复
1 回复

1,213 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

See: Booting LPC-Link 

You may also find this useful : Using the command line flash programming tool 

As far as installing a license goes, the only way to activate is via the IDE itself.

Regards,

LPCXpresso Support

0 项奖励
回复