LPC 122x ROM Bootloader using UART0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC 122x ROM Bootloader using UART0

831 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by spongehead on Wed Feb 20 17:58:16 MST 2013
On reset of LPCExpresso 122x (using LPC1227 module), if the ROM bootloader using UART0 is invoked,  does the bootloader code set the IOCONFIG  for PIO0_1 to be RXD0 and PIO0_2 to be TXD0?   Is there a way to change this without changing the bootloader code itself to use the alternate PIO2_1 (RXD0) and PIO2_2 (TXD0) pins for UART0?   Just started on using th LPC1227 module, so any input is appreciated.
0 项奖励
回复
1 回复

805 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Feb 20 18:21:55 MST 2013
You're right :) If you want different UART0 pins for ROM bootloader you've to ask NXP for your own LPC122x edition :cool:
0 项奖励
回复