JTAG Download

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JTAG Download

695件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Vit_Ciola on Fri Nov 11 11:21:20 MST 2011
It is possible to download in two microcontrollers at the same time? In other words can I record another microcontroller without cut the LPCXpresso Board?
0 件の賞賛
返信
1 返信

682件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rob65 on Sat Nov 12 00:17:49 MST 2011
No,

JTAG does not allow to place two controllers in parallel.

If you want to program another (lpc1xxx) controller without separating your board, you can just cut the traces on the PCB. Gently cut away the traces on the pins 3, 5, 7, 9 and 11 of J4. This only cuts the JTAG wires but leaves the power wires (thicker traces) in place.

Then solder a 16 pin header on the board; places jumper when you want to use this board's controller or a cable to connect to a different controller.

Please note that some controllers only support SWDIO, for those you only need the JTAG_TMS_SWDIO, JTAG_TCLK_SWCLK, JTAG_TDO_SWO and optionally the JTAG_RESET signals to be connected.

Rob
0 件の賞賛
返信