Issues with hitex_eva_4350_lpcusblib_VirtualSerialDevice example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues with hitex_eva_4350_lpcusblib_VirtualSerialDevice example

1,388 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Meyer on Wed Nov 06 08:13:15 MST 2013
Hi Lpcxpresso Team,

I tried to understand your USB application example VirtualSerialDevice, but i don´t get it run. First of all I used the lpc43xx_hitex_eva_4350_board_lib and hitex_eva_4350_usblib_device. i can compile it without errors, fine.

But if I run and plug the usb cable I got "Unknown device". If I deinstalled the Unknow device(exactly driver in Universal Serial Bus controllers)  and Unplug and plug this device again, same procedure "Unknow device"..

I have another Board (ngx_4330_xplorer) and the application example for this board no erros. I got the communication Port.


Do I need anything special note for the Hitexboard ? Anybody with the same Problem ? plz help me

Thx
0 Kudos
Reply
2 Replies

1,382 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Meyer on Fri Nov 08 00:44:54 MST 2013
Nobody with the same problem ?

Any idea´s?
0 Kudos
Reply

1,382 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Meyer on Wed Nov 06 09:05:07 MST 2013
maybe that helps
0 Kudos
Reply