Interrupt level sensitivity

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interrupt level sensitivity

740 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LynnF on Wed Apr 14 17:25:28 MST 2010
Can someone please offer an explanation of the following, please.
Edge sensitive is obvious but what is "level sensitive"? I would assume a steady state has been reached, and if correct how long is the steady state before the interrupt is generated?
[FONT=Arial][SIZE=1]
[LEFT][/SIZE][/FONT][B][FONT=Arial][SIZE=1][COLOR=#005042][FONT=Arial][SIZE=1][COLOR=#005042][FONT=Arial][SIZE=1][COLOR=#005042]Table 111. GPIOnIS register (GPIO0IS, address 0x5000 8004 to GPIO3IS, address 0x5003[/COLOR][/SIZE][/FONT][/COLOR][/SIZE][/FONT][/COLOR][/SIZE][/FONT][/B][FONT=Arial][SIZE=1][COLOR=#005042][FONT=Arial][SIZE=1][COLOR=#005042]
[B][SIZE=1][FONT=Arial][COLOR=#005042]8004) bit description[/COLOR][/FONT][/SIZE][/B]
[/COLOR][/SIZE][/FONT][/COLOR][/SIZE][/FONT][B][FONT=Arial][SIZE=1][FONT=Arial][SIZE=1]Bit Symbol Access Value Description Reset[/SIZE][/FONT][/SIZE][/FONT][/B][FONT=Arial][SIZE=1]
[B][SIZE=1][FONT=Arial]value[/FONT][/SIZE][/B]
[/SIZE][/FONT][FONT=Arial][SIZE=1][FONT=Arial][SIZE=1]11:0 ISENSE R/W Selects interrupt on pin x as level or edge sensitive[/SIZE][/FONT]
[SIZE=1][FONT=Arial](x = 0 to 11).[/FONT][/SIZE]
[SIZE=1][FONT=Arial]0x00[/FONT][/SIZE]
[SIZE=1][FONT=Arial]0 Interrupt on pin PIOn_x is configured as edge[/FONT][/SIZE]
[SIZE=1][FONT=Arial]sensitive.[/FONT][/SIZE]
[SIZE=1][FONT=Arial]1 Interrupt on pin PIOn_x is configured as [COLOR=red]level[/COLOR][/FONT][/SIZE]
[SIZE=1][FONT=Arial][COLOR=red]sensitive.[/COLOR][/FONT][/SIZE][/LEFT]
[/SIZE][/FONT]
0 Kudos
Reply
1 Reply

732 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by igorsk on Wed Apr 14 17:52:02 MST 2010
With level sensitive, you'll keep getting interrupts as long as the input remains active (low or high). With edge-sensitive it will happen only once per level transition.
0 Kudos
Reply