ISP uuencode help

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ISP uuencode help

929件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gudushen on Mon Apr 30 12:12:39 MST 2012
Can someone explain how to use ISP commands to program NXP chips?
I am having trouble understanding what exactly is being written.
For example, i try the following using hyperterminal:

[COLOR=Red]W 268439552 4[/COLOR]
0

[COLOR=Red]CATS[/COLOR]
[COLOR=Red]4[/COLOR]
1

[COLOR=Red]R 268439552 4[/COLOR]
0

$ATS@45%1

516

Why does the read gives me weird letters? it also seems to give more then 4 bytes?

Any help is greatly appreciated, an example would be best.
0 件の賞賛
返信
2 返答(返信)

911件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Fri May 04 07:12:18 MST 2012
Hi,
You didn't mention which chip you are working with, but there is an interesting app note on ISP
http://www.nxp.com/documents/application_note/AN10986.pdf
Hope you find it interesting.

Kind Regards,
0 件の賞賛
返信

911件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by researchinnovation on Wed May 02 04:34:25 MST 2012
@Gudushen...Hi...!!!

Can you please share more information about your NXP chip and project and the code which you are  using.


Thanks & Regards....:)
0 件の賞賛
返信