How to switch off Soft-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to switch off Soft-boot

1,982件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue Jun 02 06:37:21 MST 2015

Quote:
LPC-Link2 will now soft-boot with CMSIS-DAP rather than Redlink firmware by default



Unfortunately my W8.1 / Link2 needs Redlink, so where is the option to switch to Redlink  :quest:

[img=537x410]http://www.lpcware.com/system/files/DAP.jpg[/img]
0 件の賞賛
返信
2 返答(返信)

1,966件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Tue Jun 02 08:15:39 MST 2015

Quote: lpcxpresso-support
I would suspect that this is the issue with VCOM drivers...



Thanks, after updating COM17 from V1 to V2 CMSIS-DAP is working now :)
0 件の賞賛
返信

1,966件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Jun 02 07:27:00 MST 2015
So when the probe is soft-booted, if you look in Device Manager does it actually enumerate, and if so as what? I would suspect that this is the issue with VCOM drivers described in...

http://www.lpcware.com/content/faq/lpcxpresso/lpc-link2-failing-enumerate-cmsis-dap-firmware

[ Information on changing the firmware that get soft-booted will be published very shortly ]

Regards,
LPCXpresso Support
0 件の賞賛
返信