How to share PLU schematic between projects

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to share PLU schematic between projects

1,951 次查看
_Ferrari_
Contributor V

Dear all,

Im using MCUXpresso IDE v11.7.0 [Build 9198] [2023-01-17] and I developed a project, based on LPC5526 cpu, in which I used schematic tool to design PLU logic.

Now I want to reuse the same schematic and the same logic in another project based on LPC55xx processor family.

Is it possible to 'export' only the schematic and 'import' it in another project ?

thank you very much for your help and cooperation

regards

 

0 项奖励
回复
3 回复数

1,925 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @_Ferrari_ 

 

The project based on MCUXpresso IDE use the generate code from schematic, not use the schematic file, so you just need copy and paste code into your new project as XiangJun Rong said.

 

BR

Alice

 

0 项奖励
回复

1,920 次查看
_Ferrari_
Contributor V

Dear @Alice_Yang 

thank you for your email.

So it menas that it is impossible to share schematics of PLU between projects. My problem is that I have designed a schematic, and I want to import it in new project in which I have to modify it, without redraw it from scratch

0 项奖励
回复

1,914 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @_Ferrari_ 

 

"So it menas that it is impossible to share schematics of PLU between projects. My problem is that I have designed a schematic, and I want to import it in new project in which I have to modify it,"

->> What about the projects meaning? Project under MCUXpresso IDE OR PLU tool? 

 

BR

Alice

0 项奖励
回复